This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1043-Q1: WAKE 引脚问题

Part Number: TCAN1043-Q1


你好

关于TCAN1043-Q1的芯片 ,存在本地唤醒功能,关于WAKE 引脚的用法 我有一些疑问想要咨询

从图中看出 可配置成高边开关与低边配置两种方式,规格书中描述RBIAS电阻得阻值通过以下公式计算

我想问该公式是怎么计算得,电流得路径是什么?从公式推测出两个电阻是串联,但是电流回路是怎么样得呢

The RBIAS resistor is used to set the static voltage level of the WAKE pin when the switch is not in use. When the switch is in use in a high-side switch configuration, the RBIAS resistor in combination with the RSERIES resistor sets the WAKE pin voltage appropriately above the VIH threshold. The maximum value of RBIAS can be calculated using the maximum supply voltage, VSUPMAX, the maximum WAKE threshold voltage VIH, the maximum WAKE input current IIH and the series resistor value RSERIES. RBIAS is calculated using:

请协助确认以上问题

谢谢