This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCA9545A: PCA9545的电平转换问题

Part Number: PCA9545A

我在设计中使用了PCA9545和PCA9548,目前对输出I2C有几个问题。

1) SDn/SCn输出引脚是否是开漏的?

2) Datasheet中,电压转换Voltage translation用一个实例来解释,其中上游I2C总线(5V)在所有下游I2C总线(3.3V, 2.7V)中电压最高,实现了降压变换。我的问题是,上游I2C总线的电压低于下游总线的情况,也就是升压变换是否可行?例如,如果SDA/SCL输入为1.8V,所有SDn/SCn为3.3V,芯片能否正常工作?此时需要使用多大的电源电压供电?

期待您的回答。谢谢!