This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THVD2410: THVD2410何THVD2450区别

Part Number: THVD2410
Other Parts Discussed in Thread: THVD2450,

你好,

我们在使用THVD2410DR时当DE为低时,输出A无法被外部上拉的3.3V输入拉高为3.3V,只有0.6V左右。

我们做过很多次交叉验证,现象就是直接跟随芯片移动,更换一个芯片就可以恢复正常,另外我们在同样的场景和PCB上使用THVD2450,从未遇到过类似问题。

THVD2410和THVD2450是否可以混用?除了速率有区别,还有其它区别么?

实际适用速率小于500kpbs.