This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN4420: 芯片的选型和应用问题

Part Number: TCAN4420


5、物理层要求 1、通讯速率:500Kbps。 CAN控制器从外部石英晶振获取时钟源,晶振频率为CAN通讯速率的整数倍: CAN通讯速率误差:土0.2%;

2、节点ID采用扩展帧。

3、CAN总线收发器电路需要满足+8KV的接触放电不损坏。

4、CAN总线收发器电路需要满足±15KV的空气放电不损坏。

5、CAN总线收发器需要使用+5V电压进行驱动。

6、CAN总线收发器电路需要预留120的终端电阻,是否贴装TBD。

7、CAN H、CAN L与GND(动力电池)之间施加100V 1s的脉冲电压1000次, 两次之间的间隔60s,CAN 电路及通讯功能不能有损坏。

8、有超过24V电压输入/输出的节点,CAN电路需要与该电压电气隔离:

9、收发器耐压50V以上

以上要求请推荐合适的芯片.

另外“8、有超过24V电压输入/输出的节点,CAN电路需要与该电压电气隔离: ”请单独详细的说明应该怎么实现,最好有相关的参考设计或者其它详细说明,谢谢!