This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB948-Q1: 设置gpio2输出pwm给背光芯片后,背光芯片(LP8864SQRHBRQ1)输出的电20v就消失

Part Number: DS90UB948-Q1


gpio2设置为Remote GPIO Control,输出pwm给到一颗背光驱动IC(LP8864SQRHBRQ1),背光芯片(LP8864SQRHBRQ1)输出的电20v就消失了;

PWM和输出的电压,如下图红框所示:

请问可能的原因是什么?需要如何调试

  • 设置背光驱动IC(TI - LP8864SQRHBRQ1)寄存器,改为Brightness由芯片自己控制,也是会看到背光亮一下,很快输出的20V电就没有了,现象和外部pwm控制一样。

    具体寄存器设置如下:

    0x05寄存器,bit 9-8,值;2h = Brightness controlled by DISPLAY_BRT register

    0x01寄存器:值 0x7F

    0x00寄存器:值 0xFF

  • 您好

    感谢您对TI产品的关注!为更加有效地解决您的问题,我们建议您将问题发布在E2E英文技术论坛上(TI E2E support forums),将由资深的英文论坛工程师为您提供帮助