This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN4550: 芯片是否有严格的上电时序要求,目前有读写寄存器fail的情况。

Part Number: TCAN4550


供电方式目前都是通过板上供电,然后VIO通过MOS管来控制在Vsup后上电,但是看起来是晚于Vccout上电,我不确定这样会不会有问题?但是你们Spec里又写了上升时间不指定

现在芯片Vccout=5V,FLTR=1.5V,并且晶体频率也是40MHz,4分钟也能正常进入休眠模式。但是有个问题,在待机状态时,我们对同一地址的寄存器读写值不同,有时会有很多配置fail。