This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCM6208V1输出问题

有些问题想请教一下各位工程师,我设计的板卡上,CDCM6208用于给Xilinx的K7芯片提供GTX参考时钟,采用PIN_MODE 7-V1,8路时钟输出都为LVDS 125MHz。我发现,当两个GTX采用同一路时钟时,他们之间做互回环是没问题的,125M下误码率在10exp(-12)水平上。但是一旦两个GTX采用两路不同的参考时钟输入,链路误码率就会直线上升,误码率高达10exp(-6)。我初步认为是时钟同步的问题,于是在程序里给SYNCN引脚做了一个复位脉冲,维持大概2.5ms后拉高,互回环实验发现误码率仍然维持在10exp(-6)这个水平。

现在的这个误码率显然不适合做板间通信了。那么当每一路时钟输出的配置参数都相同的时候,什么因素会导致不同时钟输出链路之间的差异呢?请各位专家能够帮忙分析一下!