TI有支持16位色,TTL转LVDS的液晶屏接口芯片吗?我用的是SN65LVDS84AQ芯片,接16位色,高位悬空,为什么液晶屏显示的颜色发暗,且显示少了一块。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TI有支持16位色,TTL转LVDS的液晶屏接口芯片吗?我用的是SN65LVDS84AQ芯片,接16位色,高位悬空,为什么液晶屏显示的颜色发暗,且显示少了一块。
可是看SN65LVDS84AQ的数据手册给的电路接法是高位悬空啊。例如:12位的接法是:D4/D5,D10/D11,D16/D17悬空;那16位的接法是不是应该这样:D5/D17悬空???
你是RGB565格式?我的经验是用高位,低位悬空,也就是D0和D12悬空,我再看看啊。
你好,给你推荐一个比较符合你要求的高速率传输芯片 THCV231/236
THCV231可以将最高12Bit/pixel的LVCMOS并行信号转换为串行图像信号的发送端IC。最其具备大传输速率3.2Gbps的CML串行输出,可以将1080p60Hz的12bit摄像头图像信号通过一对双绞线或者一根同轴电缆进行传输。此外,可以通过双向的传输通道进行I2C信号传输。
THCV236/可以将THCV发送端IC输出的串行图像信号转换为最高32bit/pixel的LVCMOS并行图像信号的接受端IC。1080p60Hz的16bit的摄像头图像信号通过一对双绞线或者一根同轴电缆进行接收。此外,还具备一条可以用来传输I2C、UART或GPIO等串行信号的Sub-Link,向传输通道“Sub-Link" I2C/UART/GPIO(最高4条)
详细信息可看官网http://www.thine.co.jp/zh_cn/products/num_details/THCV231.html,我司可提供规格书、样片和技术支持,欢迎联系qq:2817821256 手机18682112448