This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA6424A的模拟IIC驱动

Other Parts Discussed in Thread: TCA6424A

BOOLEAN i2c_led_ReadData(BYTE pSrc, BYTE *pDst, UINT32 size)
{
BYTE p1 = pSrc,
*p2 = pDst;

GPIO_InitTypeDef GPIO_InitStructure;
RCC_APB2PeriphClockCmd( RCC_APB2Periph_GPIOB, ENABLE );

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP ;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOB, &GPIO_InitStructure);

if (size < 1) {return 0;} //start

Start_I2c();
SendByte(p1); //发送地址
if(ack==0)return(0);

SendByte(0x80); //发送命令字节80
if(ack==0)return(0);

Start_I2c();
SendByte(p1|0x01);//发送地址+1
if(ack==0)return(0);

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING ; 
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOB, &GPIO_InitStructure);


while (size)
{
*p2++ = i2c_RecvByte();
if (size == 1) i2c_NoAck();
else i2c_Ack();
size--;
}

Stop_I2c();
return 1;

i2c_led_ReadData(0x44,wdata084,3);

芯片地址为0x44,总TCA6424A中读出三个INPUT的数据存在数组wdata084中。

问题现象:

1、只能读出port0中的数据,命令字节不会自动增加。程序中已将命令为写成80;

2、读出来的p0的数据智能读出1位:

p01 为低电平  读出来 FE  1111 1110

p02 为低电平  读出来 FC  1111 1100

p03 为低电平  读出来 F8  1111 1000

p04 为低电平  读出来 F0  1111 0000

p05为低电平  读出来 FE  1110 0000

p06 为低电平  读出来 FC  1100 0000

p07 为低电平  读出来 F8  1000 0000

p08 为低电平  读出来 F0  0000 0000