This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TVP5158滤波器使用问题

Other Parts Discussed in Thread: TVP5158, TVP5150

使用SONY的摄像头模块(输出PAL制式),用tvp5158进行视频采集之后,发现图像质量出现以下问题:

在反差明显的竖直物体(特别是比较细的物体)边缘上容易出现彩色的偏蓝色的条纹,并且抖动厉害。

       修改tvp5158的寄存器,发现:(1)降低视频的色彩饱和度可以减轻彩色条纹,如果直接将色彩信息去除,画面只有亮度信息(即灰度图)时,彩色条纹抖动消失;(2)Luminance Processing Control 2(19h)寄存器中滤波器的选择对彩色条纹有较大影响,如果使能梳状滤波器(Luminance adaptive comb enable),或者使能陷波器(Luminance adaptive comb disable),彩色条纹比较明显,如果将梳状滤波器和陷波器都bypass(Luma comb/trap filter bypassed),则彩色条纹反而不明显;(3)对其他寄存器的修改有:Video Standard Select0Dh中将制式选择固定为(B, D, G, H, I, N) PAL,OFM Mode ControlB2h中将Out_CLK_P_En和Video_Port_En使能,Noise Reduction Control5Dh中将NR_Bypass关闭,剩下的寄存器保持默认值。

       根据上述现象,可以判断问题出现在色度和亮色分离上,有以下几个问题:

(1)为什么使用滤波器反而令彩色条纹更加严重?

       (2)Luminance Processing Control 2(19h)中所描述的梳状滤波器,是否只要使能便可以作用,还是需要设置滤波器的参数,才可以起作用?参数在哪里设置?

       图1中有通过vbus设置comb filter ram的描述,但是没有具体的说明如何设置

                                                               

    

另外在图二中tvp5150中有以下设置comb filter参数的寄存器,而在tvp5158中没有。

 

tvp5158图像质量问题描述.doc