This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB983-Q1: 983 MST模式不出图

Part Number: DS90UB983-Q1


Dear TI

           有个983 MST模式下显示黑屏问题(有一些garbge数据,但是不像是SOC输出的,把SOC刷图停到之后,garbge还存在)帮忙给一些建议。
               1. 当前调试环境:983 MST,2lane,5.4G,双1920*720,FPD-Link III
               2. 我们这边有做过一些实验:983 VP Core出pattern是正常的,问题看着在DP信号这边
               3. 对比sst和mst下 983的一些寄存器,发现有如下两个寄存器有差别,这个能说明SOC没有输出DP信号吗?
                     APB_MSA_HRES(Address:0x500,value:0x0):mst模式下异常(sst有值1920)
                     APB_MSA_VRES(Address:0x514,value:0x0):mst模式下异常(sst有值720)

               4. SOC在设置完DPRX payload id/VCPI/vc timeslot协议参数之后,有去等待DPRX的PAYLOAD_TABLE_UPDATE_STATUS (bit1:ACT Handled)置位,大概轮询了20次,983长时间无法置位。帮忙协查一下这个是什么原因?

               5. 附件是我们的983配置

BRS