只给XTR106供电,其他什么都没有接,此时输出4mA左右,可是测量14脚和6脚电压为2.05V ;13脚和6脚电压为1.5V ,和手册上的标注不太一样,连续用了两个都是这样,请问我的用法哪有错误啊
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
所描述的其他什么都没接是什么意思?那你的线路只了接Vps?
另外:
A 2.5V or 5V reference is available to excite a bridge sensor.For 5V excitation, pin 14 (VREF5) should be connected to the bridge as shown in Figure 1. For 2.5V excitation, connect pin 13 (VREF2.5) to pin 14 as shown in Figure 3b.