This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
时钟输入:
采用单端从PRIREF+输入10Mhz,PRIREF-接1K电阻接地
测试1:
Output4输出选择不经过内部VCO的LVCMOS时钟,输出是10Mhz,频率值正常,
请问:这是否可以说明外围电路供电和配置是正常的,并且Input Buffer 设置(PRI Buffer VBB,PRI Buffer Termination,input Buffer select ,AC/DC termination 等)是正确的,如果不是,在单端输入(10Mhz ,VPP=3.3V,从PRIREF+引入)的条件下应该如何选择?
测试2:
Output4输出选择经过内部VCO的时钟,设置输出频率为25Mhz时钟锁存(通过外部单片机写入,每写入一个寄存器(register0-7)后会接着把该寄存器的数读出来,结果表明数据写入都是正确的,并且unlock到EPROM里面,然后逐次上电,每次上电,Output4输出频率都不一样,23M,27M 等,测量LOck pin脚,为正脉冲信号,PLL Lock Type 为 Digital PLL Lock ,,Lock Detect Windows 3.4ns
请问,这种现象问题大概是出在什么地方了,是loop filter 还是内部VCO需要校准的缘故,能否提供一个loop filter设置的方法和原则