This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XIO3130: PCIE Switch IC XIO3130 issue.

Part Number: XIO3130

PCIE Switch IC XIO3130 issue.

we have used the chip XIO3130 in our design. The PCIe_UP_CLKP/N is 100MHz,and PCIe_UP_Nreset is high in noral operation.we also captured those two signals with oscillograph. And we also captured PCIe_UP_TXP/N(it should be RXP/N for XIO3130, and TXP/N for SoC from xilix ) waveform with oscillograph, but we can't detect the PCIe_UP_RXP/N(it should be TXP/N for XIO3130, and RXP/N for SoC from xilix ).The below pictures are the CLK signal and PCIe_UP_TXP/N sigal waveformes. We set the PCIe_UP_CLKP/N PCB trace impedence to 100Ω,PCIe_UP_TXP/N and PCIe_UP_RXP/N is 85Ω. but why XIO3130 don't send the PCIe data signals?   The below also includes the schemeatic.

  •      The below is the CLK /TX waveformes and the schematic.   

       schematic                                                                                      clk waveform    

           TX signal

  • Hi

    感谢您对TI产品的关注! 关于您的咨询,英文E2E的工程师David已经回复了这个帖子,您可以继续关注这个帖子:
    XIO3130: PCIE Switch IC XIO3130 issue

x 出现错误。请重试或与管理员联系。