This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCI2060兼容性问题?



求解用PCI2060扩展出来的PCI接口出现兼容性问题,部分PCI设备找不到(PCI网卡,PCI转串口,PCI转USB能支持,),我的设计是1转4,同步通信模式,源端由Intel南桥NM10上PCI接口引出经PCI2060转4组PCI接口,NM10的PCI支持PCI Local Bus Specification, Revision 2.3,PCI2060当前配置模式为:Intel-Compatible Mode。目前发现的不能识别的PCI设备是:Terratec Aureon5.1 PCI声卡 和 WCH:CH351Q串口,注:这两个设备如果我直接用NM10上的PCI总线是可以支持的,经过PCI2060后便识别不到了。请问是PCI2060哪里需要特殊配置还是彼此之间存在协议差异??