This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB217A: 不同电源电压会影响传输距离吗

Part Number: TUSB217A


您好,

TUSB217A  Datasheet中说VCC支持宽电源电压范围:2.3V~6.5V.

我想知道在功能配置相同的条件下,不同的供电电压会对传输距离产生影响吗?

例如:

方案A:使用5V供电,BOOST Level设置为1,RX_SEN Level设置为Medium;

方案B:使用3.3V供电,BOOST Level设置为1,RX_SEN Level设置为Medium;

在板卡生产工艺和传输线缆相同的条件下(尽量确保在相同的距离上传输损耗一致),方案A和方案B的传输距离会有差异吗?