This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCA9306: Vref1与Vref2能否可以是非同源的相同电压值?

Part Number: PCA9306

根据SPEC要求,该芯片有两种使用方式,一是EN可以接到Vref2;二是EN可以额外增加控制信号;

我只是有个疑问:这颗芯片的两端电压值可以做两个非同源但电压值相同的隔离吗?比方说Vref1=Vref2=3.3V但非同源?EN上拉至Vref2。

谢谢。

  • 您好,

    VREF1和VREF2不能是相同电压。

    VREF1和VREF2定义如下:

    VREF1:Low-voltage-side reference supply voltage for SCL1 and SDA1

    VREF2:High-voltage-side reference supply voltage for SCL2 and SDA2

    二者关系如下:

    VREF1 supports 1.2 V to VREF2 - 0.6 V. VREF2 must be between VREF1 + 0.6 V to 5.5 V.

    具体取值可以参考数据手册:

    Allows voltage-level translation between:

    – 1.2-V VREF1 and 1.8-V, 2.5-V, 3.3-V, or 5-V VREF2

    – 1.8-V VREF1 and 2.5-V, 3.3-V, or 5-V VREF2

    – 2.5-V VREF1 and 3.3-V or 5-V VREF2

    – 3.3-V VREF1 and 5-V VREF2