This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS80PCI800: 使用DS80PCI800芯片对MIPI信号进行处理改善眼图

Part Number: DS80PCI800


您好,针对DS80PCI800芯片我有一些问题,烦请解答一下,谢谢

1.想问下芯片DS80PCI800怎么确定是4lane的,我理解的lane是同时包含TX与RX两组数据,看了这块芯片的一些设计原理图发现输入和输出一般都是TX或者都是RX,所以对这方面有些疑问

2.如果要对MIPI信号进行处理,怎么确定它要设置为GEN1,GEN2还是GEN3

3.芯片的供电模式有3.3V和2.5V,这两种模式的选取有什么参考标准吗

4.由于设计的要求,可能需要用5V电压通过电平转换芯片得到需要的电压,对电平转换芯片的规格以及PCB layout有什么要求吗