This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1043HG-Q1: 功耗计算结果与datasheet差距很大,是什么问题?

Part Number: TCAN1043HG-Q1


查询功耗计算公式为:P = [(1-D)*ICCREC*VCC] + [D*ICCDOM*(VCC-VOD)] + [(1-D)*VIO*IIOREC] + (D*VIO*IIODOM) + VSUP*ISUP,按照此公式计算出的功耗为110mW,其中取值为:

  • D=50%
  • VCC=5V
  • ICCREC=5mA
  • ICCDOM=70mA
  • VOD=2.25V
  • VSUP=12V
  • ISUP=40uA
  • VIO=5V
  • IIOREC=5uA
  • IIODOM=0.45mA

datasheet中给出的功耗为58mW/126mW,请问能否给出详细的计算方法。