This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867IR: 连接路由器后,路由器端灯不亮,连接无法建立

Part Number: DP83867IR

在我的设计中共使用了两个DP83867IRRGZT芯片,两个PHY芯片的输出连接到TS3L501ERUAR的BC端口,同时TS3L501ERUAR的A端口连接RJ45,实现2选1的作用,上面是我的电路图。

默认未配置状态下,RJ45通过网线连接路由器后,路由器并没有亮灯(完全没有反应)。曾经有设计过DP83867ISRGZ,在未配置的默认状态下,RJ45通过网线连接路由器后灯会亮,路由器管理界面会检测到设备。

目前的已经发现的现象为:
正常现象:
1.在默认状态下,PHY芯片的LED输出均为高电平。
2.引脚18正确输出25M时钟
3.reset置为了高,1.8V

4.与INT_PWDN连接的电阻R183已经更改未2.2k,且电平测量为1.8V
不正常现象:
1. 3个LED在未插入网线的情况下均置为高
2.检测到TD端口出现了链路脉冲信号(P和N)


测试了之前的设计在TD端口有同样的信号
问题:
1.正常情况下reset后的状态通过网线连接RJ45至路由器是否就可以识别了,目前未识别可能是什么问题