This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB321AI: USB 接口正反插,ID和SEL管脚不会更新状态,似乎未检测到插拔

Part Number: TUSB321AI


你好:

我在使用TUSB321AI这颗芯片时遇到一个问题,我们板上用了一个typc C接口连接U盘,TUSB321AI芯片设置为DFP模式,电流设置为3A。在使用时,如果板卡上电前插入U盘,则上电后TUSB321AI能够检测到CC的信息,然后输出正常的SEL和ID信号,但是如果这时拔出U盘,再插入U盘,则SEL和ID信号则不再发生变化,这样就无法正确的识别插入方向去控制线路开关。

想咨询下这个可能是什么原因呢?

谢谢~