Part Number: DS90UB947-Q1
We wanted to replace DS90UB947T with DS90UB947N, the following issues were encountered during the use of DS90UB947-Q1:
1. What are the specific parameter differences between DS90UB947T and DS90UB947N, and what specific optimizations have DS90UB947N made on the basis of DS90UB947T?
2. I checked that these two chips are PIN to PIN compatible, can the software program used for DS90UB947T be used on the DS90UB947N without modification.
3: Whether the LVDS wiring harness used for DS90UB947T meets the standard of DS90UB947N chip, and what are the standards of DS90UB947N chip for wiring harness?