This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI,
For EMI reduction purpose, the SN65DSI83-Q1 supports the center spreading of the LVDS CLK output through the REFCLK or DSICLK input. The center spread CLK input to the REFCLK or DSI CLK is passed through to the LVDS CLK output A_CLKP/N.
If MTK platform DSI CLK only supports down spread, can SN65DSI83-Q1 support down spread?
Hello ,
down spread or center spread , that is related to spread direction.
If it is within the parameter defined for SSC_SLKIN, it is ok I think.
SN65DSI83-Q1 Automotive Single-Channel MIPI® DSI to Single-Link LVDS Bridge datasheet (Rev. A)