This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLIN1021A-Q1: TLIN1021ADRBRQ1测试

Part Number: TLIN1021A-Q1


您好:

    我们在使用TLIN1021ADRBRQ1这颗芯片时,测试SAE2602-1标准,有以下要求:

但是根据该芯片的手册,在8V供电时,LIN的最小隐性电平是0.6xVSUP=4.8V。我们实测出来在6.09V时失效,虽然在手册范围内,但是不符合SAE2602标准需要在3.29V-4.8V。

请问这个如何解释呢?谢谢。