Part Number: SN65DSI86
I used the SN65DSI86 Register calculation excel file to calculate register values for my eDP panel, but keep getting link training failed bit turned on.
Also, I'm unable to bring up the color bar test pattern.
My current hardware setup is: SDM660 -> SN65DSI86 -> eDP Panel.
The SN65DSI86_PANEL_VIDEOREGISTER_CALC.xlsm:
SN65DSI86_PANEL_VIDEOREGISTER_CALC.xlsm
This is the i2c code I'm currently using to setup the registers:
| This code is meant for an Aardvark USB to I2C to program the SN65DSI86 | ||||
| Addr | Data | |||
| <aardvark> | ||||
| <configure i2c="1" spi="1" gpio="0" tpower="1" pullups="0"/> | ||||
| <i2c_bitrate khz="100"/> | ||||
| ======ASSR RW control ====== | ||||
| <i2c_write addr="0x2D" count="1" radix="16"> | FF | 7 | </i2c_write>/> | |
| <i2c_write addr="0x2D" count="1" radix="16"> | 16 | 1 | </i2c_write>/> | |
| <i2c_write addr="0x2D" count="1" radix="16"> | FF | 0 | </i2c_write>/> | |
| ======REFCLK Frequency ====== | ||||
| <i2c_write addr="0x2D" count="1" radix="16"> | 0A | 6 | </i2c_write>/> | |
| ======DSI Mode ====== | ||||
| <i2c_write addr="0x2D" count="1" radix="16"> | 10 | 26 | </i2c_write>/> | |
| ======DSIA Clock ====== | ||||
| <i2c_write addr="0x2D" count="1" radix="16"> | 12 | 5E | </i2c_write>/> | |
| ======DSIB Clock ====== | ||||
| <i2c_write addr="0x2D" count="1" radix="16"> | 13 | 5E | </i2c_write>/> | |
| ======DP Datarate ====== | ||||
| <i2c_write addr="0x2D" count="1" radix="16"> | 94 | 80 | </i2c_write>/> | |
| ======Enable PLL ====== | ||||
| <i2c_write addr="0x2D" count="1" radix="16"> | 0D | 1 | </i2c_write> <sleep ms="10"/> | |
| ======Enable enhanced frame in DSI86 ====== | ||||
| <i2c_write addr="0x2D" count="1" radix="16"> | 5A | 4 | </i2c_write>/> | |
| ======Number of DP lanes ====== | ||||
| <i2c_write addr="0x2D" count="1" radix="16"> | 93 | 20 | </i2c_write>/> | |
| ======Start Semi-Auto Link Training ====== | ||||
| <i2c_write addr="0x2D" count="1" radix="16"> | 96 | 0A | </i2c_write> <sleep ms="20"/> | |
| ======CHA Active Line Length ====== | ||||
| <i2c_write addr="0x2D" count="2" radix="16"> | 20 | 80 | 07 | </i2c_write>/> |
| ======CHB Active Line Length ====== | ||||
| <i2c_write addr="0x2D" count="2" radix="16"> | 22 | 0 | 0 | </i2c_write>/> |
| ======Vertical Active Size ====== | ||||
| <i2c_write addr="0x2D" count="2" radix="16"> | 24 | B0 | 04 | </i2c_write>/> |
| ======Horizontal Pulse Width ====== | ||||
| <i2c_write addr="0x2D" count="2" radix="16"> | 2C | 50 | 00 | </i2c_write>/> |
| ======Vertical Pulse Width ====== | ||||
| <i2c_write addr="0x2D" count="2" radix="16"> | 30 | 04 | 00 | </i2c_write>/> |
| ======HBP ====== | ||||
| <i2c_write addr="0x2D" count="1" radix="16"> | 34 | 50 | </i2c_write>/> | |
| ======VBP ====== | ||||
| <i2c_write addr="0x2D" count="1" radix="16"> | 36 | 04 | </i2c_write>/> | |
| ===== HFP ====== | ||||
| <i2c_write addr="0x2D" count="1" radix="16"> | 38 | 50 | </i2c_write>/> | |
| ===== VFP ====== | ||||
| <i2c_write addr="0x2D" count="1" radix="16"> | 3A | 04 | </i2c_write>/> | |
| ===== DP-18BPP Disable ====== | ||||
| <i2c_write addr="0x2D" count="1" radix="16"> | 5B | 0 | </i2c_write>/> | |
| ===== Color Bar Enable ====== | ||||
| <i2c_write addr="0x2D" count="1" radix="16"> | 3C | 10 | </i2c_write>/> | |
| ===== Enhanced Frame, and Vstream Enable ====== | ||||
| <i2c_write addr="0x2D" count="1" radix="16"> | 5A | 0C | </i2c_write>/> | |
| </aardvark> | ||||
This is the i2c reg read values:
DisplayDex: read i2c addr 0x0D = 0x01
DisplayDex: read i2c addr 0x0A = 0x82
DisplayDex: read i2c addr 0x10 = 0x26
DisplayDex: read i2c addr 0x3C = 0x10
DisplayDex: read i2c addr 0x5A = 0x0C
DisplayDex: read i2c addr 0x5C = 0x11
DisplayDex: read i2c addr 0x96 = 0x00
DisplayDex: read i2c addr 0xE5 = 0x00
DisplayDex: read i2c addr 0xF0 = 0x00
DisplayDex: read i2c addr 0xF1 = 0x08
DisplayDex: read i2c addr 0xF2 = 0x00
DisplayDex: read i2c addr 0xF3 = 0x00
DisplayDex: read i2c addr 0xF4 = 0x00
DisplayDex: read i2c addr 0xF5 = 0x00
DisplayDex: read i2c addr 0xF6 = 0x00
DisplayDex: read i2c addr 0xF7 = 0x00
DisplayDex: read i2c addr 0xF8 = 0x02
this is the panel timing:


This is the hardware schematic:

Any help or hint would be much appreciated.