This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS16EV5110A: DS16EV5110A Dual Drive

Part Number: DS16EV5110A


We use two DS16EV5110A to drive DVI 2560*1600@60Hz with D0~D5 data,  however there is no phenomenon on the PC side with 2560*1600@60Hz edid parameter.

1) PC  is equipped with a GPU to support higher resolution;

2)Cable can support higher resolution than 2560*1600@60Hz;

3)Modify EDID to 1920*1080@60Hz , PC can recognize the signal,we think it works with d0~d2 data.

Attached is a schematic diagram ,thanks a lot!

  DVIIN-A.zip