Part Number: TCAN4550-Q1
I control the CANFD chip with the DSP28335 and send 5 packets of data to the outside, with the following corresponding cycle and frame ID: 0x11A, 10ms cycle; 0x11C, 20ms cycle; 0x50D, 1280ms cycle; 0x6F5, 1280ms cycle; 0x6F7, 10ms cycle. Currently, the chip's configuration is a queue size of 32. The current problem is that the data with frame ID 0x50D occasionally experiences a lost frame issue. What is the reason for this?