Other Parts Discussed in Thread: LM3477
麻烦帮我推荐一颗DCDC芯片,需求:24V转12V,输出电流5A,工作温度上线105摄氏度。
LM3477在规格书里标的1A,
网站上标的6A,麻烦解释一下。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
关于选型建议您使用官方提供的webench工具进行选择,https://webench.ti.com/power-designer/switching-regulator/select
您只需要输入参数即可生成器件对应的电路,BOM表等信息,界面供您参考,您也可以根据您的需求重新选择,
"Peak Driver Output Current"和"Iout (max) (A)"这两个概念分别代表了不同的性能指标:
Peak Driver Output Current:这个参数指的是LM3477在驱动外部MOSFET进行开关操作时,能够提供的瞬时最大电流。
Iout (max) (A) 通常指能够连续供给外部电路的最大电流。请参考。