This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,我选用了一款TI 的485收发器SN65HVD72DR,3.3V供电,总线上另外有64个5V供电的485收发器 ISL81487,这样3.3V收发器和5V收发器通信会不会有问题,目前我观察到的现象是A,B两线之间有波形,但是没有负电平,就是A的电平一直比B要高。
如果发送端的输出电平在接收端的输入电平阈值范围之内,是可以直接连接的。也就是说发送端的Voh(min)>接收端的Vih(min)。
发送端的Vol(max)<Voi(max).
查看下二者IO口的电平范围,因为3.3V TTL和5V TTL 电平阈值是相同的,如果不能直接相连,需要选择一款3.3V和5V的电平转换器件。
你好,我描述的是收发器与收发器之间的通信,不是MCU与收发器之间的通信,按照485电气规范是没有电平要求的,但是我的A,B两线是上下拉到3.3V和GND的,对面64个设备都是上下拉到5V和GND的,这两个GND是同一个地。