This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问TS3USB221A是可以放置在接口位置,进行心电信号和USB差分信号的复用,如果此芯片无法满足要求,请问有没有能够满足此应用的芯片推荐,谢谢。
ECG(心电信号)的带宽一般1000hz以内,现在需要将连接器的USB接口和心电电极引出接口进行复用,才有这样的需求,对于心电信号只要复用开关可以用于模拟信号以及复用开关本身的白噪低一些就可以,谢谢.
您好,
我建议使用 TS3USB221或 TMUXHS221、不过信号电压很重要。 TS3USB221A 可支持高达5.5V 的电压、而 TMUXHS221可支持高达3.6V 的电压。 如果它们都支持预期电压、那么我推荐这些多路复用器之一。