Other Parts Discussed in Thread: TCAN4550,
我用nrf52832的SPI来读写tcan4550.经过几天折腾,最终还是卡在了数据发送不出去的境地。
软件用的是ti的官方驱动库,初始化过程我都用log打印出来,查看都通过了。在main函数里发数据试试的,然后查询发送标志位,发现一直没反应。然后我就利用下面的函数一直读。
void tcan4550_init()
{
 /*初始化spi引脚*/
 bool error=true;
/*初始化寄存器*/
 TCAN4x5x_Device_ClearSPIERR(); // Clear any SPI ERR flags that might be set as a result of our pin mux changing during MCU startup
 nrf_delay_us(1000); 
 /* Step one attempt to clear all interrupts */
 TCAN4x5x_Device_Interrupt_Enable dev_ie = {0}; // Initialize to 0 to all bits are set to 0.
 TCAN4x5x_Device_ConfigureInterruptEnable(&dev_ie); // Disable all non-MCAN related interrupts for simplicity
TCAN4x5x_Device_Interrupts dev_ir = {0}; // Setup a new MCAN IR object for easy interrupt checking
 TCAN4x5x_Device_ReadInterrupts(&dev_ir); // Request that the struct be updated with current DEVICE (not MCAN) interrupt values
 // NRF_LOG_INFO("TCAN4x5x_Device_ReadInterrupts:%x",dev_ir.word);
 if (dev_ir.PWRON) // If the Power On interrupt flag is set
 TCAN4x5x_Device_ClearInterrupts(&dev_ir); // Clear it because if it's not cleared within ~4 minutes, it goes to sleep
/* Configure the CAN bus speeds */
 TCAN4x5x_MCAN_Nominal_Timing_Simple TCANNomTiming = {0}; // 500k arbitration with a 40 MHz crystal ((40E6 / 2) / (32 + 8) = 500E3)
 TCANNomTiming.NominalBitRatePrescaler = 2;
 TCANNomTiming.NominalTqBeforeSamplePoint = 32;
 TCANNomTiming.NominalTqAfterSamplePoint = 8;
TCAN4x5x_MCAN_Data_Timing_Simple TCANDataTiming = {0}; // 2 Mbps CAN FD with a 40 MHz crystal (40E6 / (15 + 5) = 2E6)
 TCANDataTiming.DataBitRatePrescaler = 2;
 TCANDataTiming.DataTqBeforeSamplePoint = 32;
 TCANDataTiming.DataTqAfterSamplePoint = 8;
/* Configure the MCAN core settings */
 TCAN4x5x_MCAN_CCCR_Config cccrConfig = {0}; // Remember to initialize to 0, or you'll get random garbage!
 cccrConfig.FDOE = 1; // CAN FD mode disenable
 cccrConfig.BRSE = 1; // CAN FD Bit rate switch disenable
/* Configure the default CAN packet filtering settings */
 TCAN4x5x_MCAN_Global_Filter_Configuration gfc = {0};
 gfc.RRFE = 1; // Reject remote frames (TCAN4x5x doesn't support this)
 gfc.RRFS = 1; // Reject remote frames (TCAN4x5x doesn't support this)
 gfc.ANFE = TCAN4x5x_GFC_ACCEPT_INTO_RXFIFO0; // Default behavior if incoming message doesn't match a filter is to accept into RXFIO0 for extended ID messages (29 bit IDs)
 gfc.ANFS = TCAN4x5x_GFC_ACCEPT_INTO_RXFIFO0; // Default behavior if incoming message doesn't match a filter is to accept into RXFIO0 for standard ID messages (11 bit IDs)
/* ************************************************************************
 * In the next configuration block, we will set the MCAN core up to have:
 * - 1 SID filter element
 * - 1 XID Filter element
 * - 5 RX FIFO 0 elements
 * - RX FIFO 0 supports data payloads up to 64 bytes
 * - RX FIFO 1 and RX Buffer will not have any elements, but we still set their data payload sizes, even though it's not required
 * - No TX Event FIFOs
 * - 2 Transmit buffers supporting up to 64 bytes of data payload
 */
 TCAN4x5x_MRAM_Config MRAMConfiguration = {0};
 MRAMConfiguration.SIDNumElements = 1; // Standard ID number of elements, you MUST have a filter written to MRAM for each element defined
 MRAMConfiguration.XIDNumElements = 1; // Extended ID number of elements, you MUST have a filter written to MRAM for each element defined
 MRAMConfiguration.Rx0NumElements = 5; // RX0 Number of elements
 MRAMConfiguration.Rx0ElementSize = MRAM_64_Byte_Data; // RX0 data payload size
 MRAMConfiguration.Rx1NumElements = 0; // RX1 number of elements
 MRAMConfiguration.Rx1ElementSize = MRAM_64_Byte_Data; // RX1 data payload size
 MRAMConfiguration.RxBufNumElements = 0; // RX buffer number of elements
 MRAMConfiguration.RxBufElementSize = MRAM_64_Byte_Data; // RX buffer data payload size
 MRAMConfiguration.TxEventFIFONumElements = 0; // TX Event FIFO number of elements
 MRAMConfiguration.TxBufferNumElements = 2; // TX buffer number of elements
 MRAMConfiguration.TxBufferElementSize = MRAM_64_Byte_Data; // TX buffer data payload size
 /* Configure the MCAN core with the settings above, the changes in this block are write protected registers, *
 * so it makes the most sense to do them all at once, so we only unlock and lock once */
error = TCAN4x5x_MCAN_EnableProtectedRegisters(); // Start by making protected registers accessible
 NRF_LOG_INFO("TCAN4x5x_MCAN_EnableProtectedRegisters:%d",error);
 error =TCAN4x5x_MCAN_ConfigureCCCRRegister(&cccrConfig); // Enable FD mode and Bit rate switching
 NRF_LOG_INFO("TCAN4x5x_MCAN_ConfigureCCCRRegister:%d",error);
 error =TCAN4x5x_MCAN_ConfigureGlobalFilter(&gfc); // Configure the global filter configuration (Default CAN message behavior)
 NRF_LOG_INFO("TCAN4x5x_MCAN_ConfigureGlobalFilter:%d",error);
 error =TCAN4x5x_MCAN_ConfigureNominalTiming_Simple(&TCANNomTiming);// Setup nominal/arbitration bit timing
 NRF_LOG_INFO("TCAN4x5x_MCAN_ConfigureNominalTiming_Simple:%d",error);
 error =TCAN4x5x_MCAN_ConfigureDataTiming_Simple(&TCANDataTiming); // Setup CAN FD timing
 NRF_LOG_INFO("TCAN4x5x_MCAN_ConfigureDataTiming_Simple:%d",error); 
 TCAN4x5x_MRAM_Clear(); // Clear all of MRAM (Writes 0's to all of it)
 error =TCAN4x5x_MRAM_Configure(&MRAMConfiguration); // Set up the applicable registers related to MRAM configuration
 NRF_LOG_INFO("TCAN4x5x_MRAM_Configure:%d",error);
 
 error = TCAN4x5x_TimeStampDisable();
 NRF_LOG_INFO("TCAN4x5x_TimeStampDisable:%d",error);
 
 //error = TCAN4x5x_LoopbackModeEnable();
 //NRF_LOG_INFO("TCAN4x5x_LoopbackModeEnable:%d",error);
 
 error =TCAN4x5x_MCAN_DisableProtectedRegisters(); // Disable protected write and take device out of INIT mode
 NRF_LOG_INFO("TCAN4x5x_MCAN_DisableProtectedRegisters:%d",error);
/* Set the interrupts we want to enable for MCAN */
 TCAN4x5x_MCAN_Interrupt_Enable mcan_ie = {0}; // Remember to initialize to 0, or you'll get random garbage!
 mcan_ie.RF0NE = 1; // RX FIFO 0 new message interrupt enable
 mcan_ie.TCE = 1;
 TCAN4x5x_MCAN_ConfigureInterruptEnable(&mcan_ie); // Enable the appropriate registers
 /* Setup filters, this filter will mark any message with ID 0x055 as a priority message */
 TCAN4x5x_MCAN_SID_Filter SID_ID = {0};
 SID_ID.SFT = TCAN4x5x_SID_SFT_CLASSIC; // SFT: Standard filter type. Configured as a classic filter
 SID_ID.SFEC = TCAN4x5x_SID_SFEC_PRIORITYSTORERX0; // Standard filter element configuration, store it in RX fifo 0 as a priority message
 SID_ID.SFID1 = 0x055; // SFID1 (Classic mode Filter)
 SID_ID.SFID2 = 0x7FF; // SFID2 (Classic mode Mask)
 error =TCAN4x5x_MCAN_WriteSIDFilter(0, &SID_ID); // Write to the MRAM
 NRF_LOG_INFO("TCAN4x5x_MCAN_WriteSIDFilter:%d",error);
/* Store ID 0x12345678 as a priority message */
 TCAN4x5x_MCAN_XID_Filter XID_ID = {0};
 XID_ID.EFT = TCAN4x5x_XID_EFT_CLASSIC; // EFT
 XID_ID.EFEC = TCAN4x5x_XID_EFEC_PRIORITYSTORERX0; // EFEC
 XID_ID.EFID1 = 0x12345678; // EFID1 (Classic mode filter)
 XID_ID.EFID2 = 0x1FFFFFFF; // EFID2 (Classic mode mask)
 error =TCAN4x5x_MCAN_WriteXIDFilter(0, &XID_ID); // Write to the MRAM
 NRF_LOG_INFO("TCAN4x5x_MCAN_WriteXIDFilter:%d",error);
 /* Configure the TCAN4550 Non-CAN-related functions */
 TCAN4x5x_DEV_CONFIG devConfig = {0}; // Remember to initialize to 0, or you'll get random garbage!
 devConfig.SWE_DIS = 0; // Keep Sleep Wake Error Enabled (it's a disable bit, not an enable)
 devConfig.DEVICE_RESET = 0; // Not requesting a software reset
 devConfig.WD_EN = 0; // Watchdog disabled
 devConfig.nWKRQ_CONFIG = 0; // Mirror INH function (default)
 devConfig.INH_DIS = 0; // INH enabled (default)
 devConfig.GPIO1_GPO_CONFIG = TCAN4x5x_DEV_CONFIG_GPO1_MCAN_INT1; // MCAN nINT 1 (default)
 devConfig.FAIL_SAFE_EN = 0; // Failsafe disabled (default)
 devConfig.GPIO1_CONFIG = TCAN4x5x_DEV_CONFIG_GPIO1_CONFIG_GPO; // GPIO set as GPO (Default)
 devConfig.WD_ACTION = TCAN4x5x_DEV_CONFIG_WDT_ACTION_nINT; // Watchdog set an interrupt (default)
 devConfig.WD_BIT_RESET = 0; // Don't reset the watchdog
 devConfig.nWKRQ_VOLTAGE = 0; // Set nWKRQ to internal voltage rail (default)
 devConfig.GPO2_CONFIG = TCAN4x5x_DEV_CONFIG_GPO2_NO_ACTION; // GPO2 has no behavior (default)
 devConfig.CLK_REF = 1; // Input crystal is a 40 MHz crystal (default)
 devConfig.WAKE_CONFIG = TCAN4x5x_DEV_CONFIG_WAKE_BOTH_EDGES;// Wake pin can be triggered by either edge (default)
 error =TCAN4x5x_Device_Configure(&devConfig); // Configure the device with the above configuration
 NRF_LOG_INFO("TCAN4x5x_Device_Configure:%d",error);
 
 
 error =TCAN4x5x_Device_SetMode(TCAN4x5x_DEVICE_MODE_STANDBY); // Set to normal mode, since configuration is done. This line turns on the transceiver
 NRF_LOG_INFO("TCAN4x5x_Device_SetMode:%d",error);
 
 error =TCAN4x5x_Device_SetMode(TCAN4x5x_DEVICE_MODE_NORMAL); // Set to normal mode, since configuration is done. This line turns on the transceiver
 NRF_LOG_INFO("TCAN4x5x_Device_SetMode:%d",error);
 
 TCAN4x5x_MCAN_ClearInterruptsAll(); // Resets all MCAN interrupts (does NOT include any SPIERR interrupts) 
}
void tcan4550_data_tx(void)
{
 TCAN4x5x_Device_Interrupts dev_ir = {0}; // Define a new Device IR object for device (non-CAN) interrupt checking
 TCAN4x5x_MCAN_Interrupts mcan_ir = {0}; 
 
 /* Define the CAN message we want to send*/
 TCAN4x5x_MCAN_TX_Header header = {0}; // Remember to initialize to 0, or you'll get random garbage!
 uint8_t data[8] = {0x55, 0x66, 0x77, 0x88,0x99, 0xaa, 0xbb, 0xcc}; // Define the data payload
 header.DLC = MCAN_DLC_8B; // Set the DLC to be equal to or less than the data payload (it is ok to pass a 64 byte data array into the WriteTXFIFO function if your DLC is 8 bytes, only the first 8 bytes will be read)
 header.ID = 0x144; // Set the ID
 header.FDF = 0; // CAN FD frame enabled
 header.BRS = 0; // Bit rate switch enabled
 header.EFC = 0;
 header.MM = 0;
 header.RTR = 0;
 header.XTD = 0; // We are not using an extended ID in this example
 header.ESI = 0; // Error state indicator
 
 TCAN4x5x_MCAN_WriteTXBuffer(0, &header, data); // This function actually writes the header and data payload to the TCAN's MRAM in the specified TX queue number. It returns the bit necessary to write to TXBAR,
 // but does not necessarily require you to use it. In this example, we won't, so that we can send the data queued up at a later point.
/* Let's make a different CAN message */
 data[0] = 0x11;
 data[1] = 0x22;
 data[2] = 0x33;
 data[3] = 0x44; // Define the data payload
header.DLC = MCAN_DLC_8B; // Set the DLC to be equal to or less than the data payload (it is ok to pass a 64 byte data array into the WriteTXFIFO function if your DLC is 8 bytes, only the first 8 bytes will be read)
 header.ID = 0x123; // Set the ID
 header.FDF = 0; // CAN FD frame enabled
 header.BRS = 0; // Bit rate switch enabled
 header.EFC = 0;
 header.MM = 0;
 header.RTR = 0;
 header.XTD = 0; // We are not using an extended ID in this example
 header.ESI = 0; // Error state indicator
TCAN4x5x_MCAN_WriteTXBuffer(1, &header, data); // This line writes the data and header to TX FIFO 1
TCAN4x5x_MCAN_TransmitBufferContents(1); // Request that TX Buffer 1 be transmitted
 nrf_delay_ms(100); 
 NRF_LOG_INFO("AddRequestTransmission1:%X",TCAN4x5x_MCAN_Tx_AddRequestTransmissionOccurred(1));
 TCAN4x5x_Device_ReadInterrupts(&dev_ir); 
 TCAN4x5x_MCAN_ReadInterrupts(&mcan_ir); 
 
 //while(!mcan_ir.TC);
 NRF_LOG_INFO("Device_ReadInterrupts:%X",dev_ir.word);
 NRF_LOG_INFO("MCAN_ReadInterrupts:%X",mcan_ir.word);
 NRF_LOG_INFO("MCAN_ReadInterruptsflag:%X",AHB_READ_32(0x0824));
 // TCAN4x5x_MCAN_ClearInterruptsAll(); 
}
logo输出的结果是这样的


硬件电路图是这样的

SPI的四根线跟主控链接,VSUP 5V,VIO3.3V。
TCAN4550canl 和canH接到can逻辑分析仪。
疑问1:现在没啥思路继续排查问题,请问下个方向我如何做呢?
疑问2:我自己做过另一个集成主控和tcan4550的小板子,发现同样的程序spi只能把ID给读出来,可是写其他寄存器就失败,读出来都是0。这也是一头雾水?
请帮忙指点一下方向。