跪求大牛
我正在使用的一片LMK03806,当上电运行一段时间后,有时二十分钟有时会更长时间,其中从VCO出来的时钟相对于Buffer出来(参考时钟的buffer)的时钟的相位相对于上电时会发生90度或180的跳变!百思不得其解,为什啊???!!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
跪求大牛
我正在使用的一片LMK03806,当上电运行一段时间后,有时二十分钟有时会更长时间,其中从VCO出来的时钟相对于Buffer出来(参考时钟的buffer)的时钟的相位相对于上电时会发生90度或180的跳变!百思不得其解,为什啊???!!!
用具有差分探头的高速示波器测的,一头点在参考时钟,另一头输出时钟
参考是125M,VCO锁到2.5G
我可不是大牛
我感觉象失锁后重新又锁定了照成的相位随机变化
再过20分钟还会再发生相位变化吗?
环路滤波器是 C1 = 220 pF, C2 = 18 nF, R2 = 820 Ω,, C3 = 10 pF, R3 = 200 Ω, C4 = 10 pF, R4 = 200 Ω还可以?
其次是R26[29]=‘1’--Reference frequency doubled (2x),R29[22:5]=80---PLL_N_CAL这个地方还有问题
我实在想不到哪里会导致失锁?
谢谢!!