求助TI
目前我调试两路sensor;
1,914->913->sensor,这路目前已经正常。
2,940->913->sensor,这路出现问题,目前读940的寄存器,在REMOTE ID(0x07)中没有lock到Serializer 913的ID,该寄存器为00。不知是否可以用这种方案。在940 的General Status(0x1C)寄存器中,值为0x22,表明SIGNAL DETECT为1,LOCK为0.说明是检测到串行输入。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
940 是CSI输出,而913是LVCMOS输入,二者接口不同啊,而914的输出也是LVCMOS输出,所以可以和913搭配使用。
不知道你为什么913和940搭配使用,可以看下二者的架构,913是单差分对输出,而940是双差分对输入,是因为CPU接口有CSI接口,需要940这款吗?为什么不使用914和913搭配?I believe 说:我们的数据是这样的,sensor->913->940->cpu,940和913 用FPD-LinkIII
接口电平不同,是不能直接连接的。I believe 说:你好!Kailyn,
你的意思是无论怎么使用,940和913因为输入输出的接口不匹配,所以不能配对使用么
你好!Kailyn,
现将我们产品的应用设计跟您明确一下:
我们产品是要用到双摄像头方案,同时我们选用的CPU的sensor接口目前只支持1个并行接口和1个CSI-2接口。摄像头模组采用8/10bit并行接口。
但因我们实际的应用环境和产品结构设计,摄像头离CPU比较远,因此我们考虑采用1对串行和解串器来增加传输长度。
针对并行接口,我们采用的是913和914芯片,即连接方式是:sensor(并行)-913-914-CPU(并行)
针对CSI-2接口,我们采用913和940芯片,即连接方式是:sensor(并行)-913-940-CPU(CSI-2)。其中,913通过lvcmos并行与sensor连接,913和940通过fpd-linkIII连接,940的输出CSI-2接口连至CPU的CSI-2输入接口上。
目前。sensor(并行)-913-914-CPU(并行)这组通路已经调通,CPU已可以采集到摄像头数据。
而现在问题是:sensor(并行)-913-940-CPU(CSI-2)这组通路不通,具体表现在,CPU可以通过I2C访问940,但CPU无法透过940去访问913的寄存器,似乎CPU-940-913这个通路之间存在问题。
现在我们不确定的是940和913能否配对使用,因为从典型应用来看,940好像没有何913这么接过。但从电平标准上看,因为940和913相连的接口都是fpd-link,似乎应该没什么问题。
因此请帮忙确认,940和913能否配对使用,如果可以的话,那么我们是不是940寄存器的配置还存在一些问题,导致通路没配通,请帮忙指出,谢谢!
我看了下这个方向是可以的:sensor->913->940->cpu,940和913 用FPD-LinkIII
940可以配置多种模式,可以采用1 lane FPD-Link III Input,将RIN1disable掉,输出你再配置成2 MIPI lanes输出还是4 MIPI lanes output。你可以参考下940 datasheet的Page35。
而你之前说的940-913-sensor这个方向,940输出CSI接口,而913是LVCMOS,二者电平不匹配