This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN4550-Q1: 正常使用1~3小时后,无法发送数据

Part Number: TCAN4550-Q1


您好!

我们设备上用一个SPI上挂了两个TCAN4550-Q1芯片,通过片选来切换通讯,出现问题如下:

现象:1、设备出现使用1到3小时左右,CAN1随机时刻出现无法发出数据到CAN总线上,但是可以正常接收CAN总线上数据,CAN2收发都正常;

           2、CAN1无法发数据的时候,内核没有任何报错,将CAN1重新初始化下,又可正常使用;

           3、多台设备出现相同现象

原理图如下: