This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB216: TUSB216 DM/DP管脚是否支持反转

Part Number: TUSB216


Hi   Ti expert

当前在使用TUSB216作为USB2.0 redriver遇到问题。请问:

1.TUSB216 内部是否为纯硬件线路,不包含协议内容,DM/DP管脚内部结构是完全一样的;

2.如果USB DN信号在TSUB216前后都连接在了DP管脚,USB DP信号连接到了DM管脚,这样前后同步调换DP/DN管脚是否OK。

谢谢。

  • 1.所有的硬件都在内部。没有软件用于HS检测或类似的事情。

    2.DN和DP应连接到各自的引脚,DN不应连接到DP引脚,反之亦然。同步调换是什么意思?比如,DN连接到DN1,然后切换到DP2?或者你的意思是认为DN在重新驱动后成为DP?

  • 不是DP和DN信号交叉,是如下图这样,信号名为DN的信号连接在了D1P和D2P的管脚上,信号名为DP的信号连接在了D1M和D2M的管脚上。如果TUSB216是一个单纯的redriver器件的话,不涉及协议的话,这样连接是否也是可以的。

  • DP应连接到DP引脚,DN应连接到DN引脚。我们不建议反转极性。

    TUSB216是一个双向redriver,因此如果需要,可以转动redriver,使DP和DN引脚与正确的通道对齐。

  • 正常的设计肯定是按照正确的极性连接,现状是设计的时候连接错误了,我们有咨询一些其他厂商,他们反馈纯硬件的redriver他们支持这种连接方法,DP,DN管脚在芯片内部结构是完全一样的,所以只要芯片前后信号统一就可以。所以想确认的是TUSB216是否支持这样的连接。

  • 对于此设备,DP和DN需要连接到正确的引脚,因为它需要能够检测DP和DN线路特有的上拉。如果它没有正确检测到这个上拉,它将无法正确启用。