This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB913A的传输距离

请问DS90UB913A的传输距离有多少?

  • 传输距离和很多因素有关,在数据手册上也提到了:

    The maximum length of cable that can be used is dependent on the quality of the cable (gauge, impedance), connector, board(discontinuities, power plane), the electrical environment (for example, power stability, ground noise, input clock jitter, PCLK frequency, etc).

    目前你需要传输的距离为多少?为了保证信号的完整性,如果传输距离太长,需要加均衡器的

  • 你好,给你推荐一个型号THCV231/236,具备大传输速率3.2Gbps,现在实测距离是12米,要看你想达到什么样的效果,THCV235/236可以传输更远,

    THCV231可以将最高12Bit/pixel的LVCMOS并行信号转换为串行图像信号的发送端IC。最其具备大传输速率3.2Gbps的CML串行输出,可以将1080p60Hz的12bit摄像头图像信号通过一对双绞线或者一根同轴电缆进行传输。此外,可以通过双向的传输通道进行I2C信号传输。

    THCV236/可以将THCV发送端IC输出的串行图像信号转换为最高32bit/pixel的LVCMOS并行图像信号的接受端IC。1080p60Hz的16bit的摄像头图像信号通过一对双绞线或者一根同轴电缆进行接收。此外,还具备一条可以用来传输I2C、UART或GPIO等串行信号的Sub-Link,向传输通道“Sub-Link"  I2C/UART/GPIO(最高4条)

    详细信息可看官网http://www.thine.co.jp/zh_cn/products/num_details/THCV231.html,我司可提供规格书、样片和技术支持,欢迎联系qq:2817821256 手机18682112448