1、LMK01010和LMK01020的BIAS管脚是接100nF上拉到VCC呢还是接1uF上拉到VCC?
2、接问题1,当BIAS管脚经过电容上拉到VCC后,对LMK01010和LMK01020有什么影响?是不是输出的LVDS(LMK01010)、LVPECL(LMK01020)的直流偏置电路无效了,需要在输出端口外接直流偏置电路吗?如果接收器内部有自偏压电路,并且兼容LVDS和LVPECL,譬如AD9957的ref_clk该怎样进行交流匹配,耦合电容为0.1uF
多谢!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1、LMK01010和LMK01020的BIAS管脚是接100nF上拉到VCC呢还是接1uF上拉到VCC?
A: bias需要接1uF电容上拉到VCC。
datasheet中的Figure2,bias是通过100nF电容上拉到Vcc,这里的100nF应该是1uF才对。
2、接问题1,当BIAS管脚经过电容上拉到VCC后,对LMK01010和LMK01020有什么影响? A:bias经过1uF电容上拉到Vcc的作用,在datasheet里有描述: To properly use the device, bypass Bias (pin 36) with a low leakage 1 μF capacitor connected to Vcc. This is important for low noise performance.
Q: 是不是输出的LVDS(LMK01010)、LVPECL(LMK01020)的直流偏置电路无效了,需要在输出端口外接直流偏置电路吗?如果接收器内部有自偏压电路,并且兼容LVDS和LVPECL,譬如AD9957的ref_clk该怎样进行交流匹配,耦合电容为0.1uF
A: 有效的,正因为LMK01010 本身已经提供了有效的偏置电路,所以在和接收端进行耦合时,要看接收端内部是否也有偏置电路,如果没有的话,建议DC耦合,如果已经有了偏置电路,则AC耦合便可。
如果LMK01020和LMK01010的bias管脚接100nF下拉到GND,会对器件的性能有多大的影响?是否会影响器件的长期可靠性?按照回复,LMK01020和LMK01010的输出都是有内置的偏压电路的,对吧?内置的偏压电路会受到BIAS管脚的影响吗?因为器件资料对BIAS管脚的描述是“bypass bias”——“旁路偏置”,个人以为是bias管脚上接不同的电路会影响器件的输出的偏置电路,希望您不厌其烦地给予解答,万分感谢!
接0.1uF或者接1uF应该对性能影响不大。
是的,这两款内部都有偏置电路。 Bias引脚接电容到Vcc主要是考虑噪音方面的影响。