This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
There are some issues with using the AUX function of DS90UH983. When measuring with an oscilloscope, it was found that the HPD signal was raised, but there was no signal on the AUX. May I ask which registers need to be configured before using the AUX of DS90UH983?
Hi ,
Who is the tier 1 and OEM?
No registers need to be configured for AUX communication - the source (i.e. SoC) should start sending AUX transaction upon detection of HPD from the sync device (i.e. 983).
Are you able to provide any additional context on this issue (i.e. SoC utilized, DP vs. eDP configuration, number of cycles needed to observe a failure, etc.)?
Also, where in the system is the probe being placed to read the AUX signal? Depending on where the probe is placed, the AUX electrical specifications may change.
Best,
Links