This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教,DS90UB914无法正常解出PCLK,HS,VS信号!



你好!

我司的车载项目,DS90UB913可以检测到正常的CLK, HS, VS,LVDS(见附件)信号,但是在接收端914无法正常解出PCLK, HS,VS,测试各电压和电路设置均正常!请帮忙看看附件原理图分析下原因,谢谢!

MobileFile.rar
  • 913和914均采用默认设置,没有受控,二边的DATA接口均为:D2-D9

  • Mr. Wu

    根据你的描述,UB914应当内部的CDR应当没锁定。为了简化定位,使用BIST模式,具体请查阅UB914中关于BIST的详细介绍。

    这样就把问题局限在UB913、接插件、线缆、UB914中间。

    1. 使用标准的焊接在单板上的接插件和长度0.5米以内的STP线缆,排除接插件和线缆带来的问题。 这里严重不推荐使用非标的线缆,直接焊接在高速过孔上。

    2. 启用BIST,检查pass 管脚或者内部的误码率寄存器。

    谢谢

  • 你好,给你推荐一个比较符合你要求的高速率传输芯片  THCV231/236 

    THCV231可以将最高12Bit/pixel的LVCMOS并行信号转换为串行图像信号的发送端IC。最其具备大传输速率3.2Gbps的CML串行输出,可以将1080p60Hz的12bit摄像头图像信号通过一对双绞线或者一根同轴电缆进行传输。此外,可以通过双向的传输通道进行I2C信号传输。

    THCV236/可以将THCV发送端IC输出的串行图像信号转换为最高32bit/pixel的LVCMOS并行图像信号的接受端IC。1080p60Hz的16bit的摄像头图像信号通过一对双绞线或者一根同轴电缆进行接收。此外,还具备一条可以用来传输I2C、UART或GPIO等串行信号的Sub-Link,向传输通道“Sub-Link"  I2C/UART/GPIO(最高4条)

    详细信息可看官网http://www.thine.co.jp/zh_cn/products/num_details/THCV231.html,我司可提供规格书、样片和技术支持,欢迎联系qq:2817821256 手机18682112448