This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
文章第11页
在无SCCP进行通信的情况下,PSE是如何检测PD并分类供电的?在IEEE802.3CG和IEEE802.3BU这两篇文档中未找到不经过SCCP进行分类检测就供电的具体流程说明。看常规检测流程是PSE将PI总线拉高至4.7V附近,然后检测到电流在9-16ma便认为设备已经接上。如果不启用SCCP分类的话就直接开始供电么,看802.3描述如果不经过分类就按照默认的class0来供电,因此观察绿色的线推测你们将输出拉高至class0规定的最高18V电压,我的理解对么?
您有两种选择可以符合IEEE标准,要么使用SCCP进行PoDL,要么不使用SCCP。如果不这样做,PSE将启用9-16mA的电流源,并检查电压是否升至约4V。如果是这样,可以启用全电源电压。
希望这有助于理解。
感谢您的回答。请问不使用SCCP的相关流程有IEEE的具体文章进行说明么。参考上面的截图(snla395),我对3V 、1.25mA 、1.85mA 、12mA 、4V这些特定数值比较疑惑。我看802.3cg中写道
PSE的开路电压为4.75-5.5V,但在snla395中看到你们给的起始电压为3V,两者并不符合,可否给个具体说明,或者告诉我IEEE的标准化文件具体哪一篇有相关说明。感谢