This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB983-Q1: dp->943->948 系统小概率闪屏,异常的时读到page_12 0x31寄存器bit4被设置成1。

Part Number: DS90UB983-Q1


INTR_STS_VP_VP0 Register (Address = 0x31) [Default = 0x0]  寄存器在异常时 bit4被置位。

IS_TIMING_DATA_ERR 0x0 Timing Gen Data Available error
This error is reported if the timing generator detects a line length
error or other error that results in no data available to send from the
video buffer during active horizontal period.

请问在哪种情况下这个bit会被设置1

  • 您好 已经收到了您的案例,调查需要些时间,感谢您的耐心等待

  • 您好

    谁是第1级和 OEM?

    很乐意就此问题提供支持、但我需要一些额外的背景信息、以便更好地了解正在发生的事情。

    请参阅以下内容:

    在总共多少个器件中、有多少个器件会产生影响?

    如果是多个、是否已执行 ABA 交换?

    重新出现该问题需要多少次下电上电?

    显示屏的时序参数(有效和消隐)是什么?

    什么是"启动界面"?

    您可以收集983的一个良好的 NG 寄存器转储、特别是在主页、第12页和 APB 页上?