Part Number: TCAN1146-Q1
在TJA1145ATK的数据表中,有“输入对地电容(CANH或CANL)”,其最大值为20pF
我能知道哪种CAN收发器可以满足对地输入电容最大值(CANH或CANL)低于20pf的要求吗?
In the datasheet of TJA1145ATK, there is "Input capacitance to Ground (CANH or CANL)" , and the max value of it is 20pF
Could I konw which CAN transceiver could meet the requirement that max value of input capacitance to Ground (CANH or CANL) is below 20pf ?