This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
从芯片手册中可以看到,外部信号进入芯片后,会经过R1,R2分压,分压后的值输入芯片内部的比较器,判断高低。如果芯片外部串联电阻Rin,输入电压先经过Rin,R1,R2分压,再到芯片内部比较器比较,判断输入的高低。这种情况下,Rin值得选取会影响芯片判断高,低的阈值。请问我的理解对吗?请举例说明下,如果外部串联了510欧姆电阻,对芯片阈值得影响。
谢谢!
您好,
是的,RIN电阻上会有压降(8.3.8.1 Input Current Source and Sink Selection)。
请参考“8.3.8.3 Thresholds Adjustment”设置阈值。
您好,没有理解8.3.8.3。如果选定阈值为4V,湿润电流为10mA,输入电压VBAT为0~16V,串联RIN为510Ω,请帮忙计算下,VBAT为多少伏,INx判断为高;VBAT为多少伏,INx判断为低,请帮忙列一下计算公式。
您好,
基本电压计算基于欧姆定律 (V=I*R)。因此,首先计算电阻器和开关总串联电阻上的电压降,然后从 VBAT 电压中减去该电压。
VINx = VBAT - (Iwett * Rtotal)
或:
VINx = VBAT - (Iwett * (RIN + RSW))