This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA9803: 低温-20℃情况下I2C报错

Part Number: TCA9803
Other Parts Discussed in Thread: TCA9406, TCA39306, PCA9306, , TCA9416

低温-20℃情况下I2C报错,常温没问题,每台机器出现的概率100%

1、示波器接SDA B\SCL B端发现SDA信号没有应答位错误。主机发送数据给从机后,应答位SDA没有释放的动作,波形上没有应答为之前的主机释放从机拉低的尖峰动作。

2、示波器探头点到SDA A端,I2C报错就会消失;探头一松开,I2C报错就会出现;探头再一点上去,I2C就又会报错。所以SDA A\SCL A端的错误波形无论如何都抓不到。

3、SDA A芯片脚上无论焊接一端浮空的线或者一端浮空的电容,低温下I2C报错消失,用电烙铁取下后,报错现象永久消失。

4、通过增加芯片所在板和主板之间的FPC排线长度;增大SDA A\SCL A端的上拉电阻为10k;SDA A\SCL A端加一个10pF的对地电容。这三个措施的任意一个都可以解决低温下I2C报错的问题。

请问一下,以上低温下I2C报错的原因是什么?

  • 感谢您对TI产品的关注!
    关于你的咨询,我们正在确认你的问题,稍后回复您。

  • This is a difficult issue to debug with merely words and no evidence in a scope capture. I understand that it cannot be captured, but it is interesting that the issue goes away once the probe touches the I2C bus. Adding a probe would add some parasitic capacitance to the bus.
    Do we have a schematic to review?
    What is the input low voltage on VILA and VILB?
  • TCA9803缓冲区的B侧连接了哪些其他设备/外围设备?是否有TCA39306/PCA9306/TCA9406/TCA9416/等无源电平转换装置。?
    我们如何确定TCA9803将巴士保持在锁定状态?客户如何确定TCA9803是问题所在,而不是缓冲器B侧的其他设备?

  • B侧只接了一个传感器,没有接任何其他器件。

    1.A侧是ARM,B侧是传感器,中间就接了一个TCA9803。一般情况下我们的项目是A直接连B,但此项目1.8V的i2c不够,所以就加了9803,这种项目我们每年会做几十万台机器,没有出现过低温下i2c报错。但加上了9803的几十台机器100% i2c报错。

    2.我们其他部门之前也用了这个器件做隔离,也说低温下器件很敏感,后面取消9803,直接用串阻连接在一起就好了。

    3.我们的这个9803在单独一个板子上,A侧ARM在一个板子上,B侧传感器在另一个板子上,只有在9803这个板子上的I2C数据线上飞线或者焊接,然后把飞线取下来后,问题就不复现了。而在其他两块板子上焊接器件,取下来后,低温问题现象依旧复现。

  • 整个系统是否处于低温(-20℃),还是只有TCA9803在-20℃下通过热流?
    我们还可以确认电阻器R1181和R1182是否已去填充?如果这些电阻器没有填充,那么原理图看起来不错。
    B侧使用的是什么传感器?我们如何知道B侧的传感器不是在低温下保持总线低电平的设备?

  • 整个系统全都处于低温-20℃;R1182和R1181去填充,没有上键;B侧使用的传感器是红外热成像探测器;当i2c的io直连探测器时,不会出现低温下报错,加了9803后才会出现报错

  • 这个问题没有意义。
    解决这个问题的o-scope探头似乎不起作用。o-scope探头会给I2C增加一些泄漏,但应该非常小。是否仅在测试期间将示波器探头添加到A侧?只有当B侧连接了o-scope探头时,问题才会消失吗?
    示波器探头可能会增加10-15pF的电容,这会略微减缓上升时间。客户是否在-20℃的相同条件下使用TCA9803进行了测试,但数据速率稍慢?如果它们以400kHz运行,请尝试390kHz,看看问题是否已解决?也许是时间问题?
    我们是否有一个工作案例的范围捕获,以便我们可以分析波形的VOL和上升时间?我们能从范围上衡量这一点吗?