This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867IR: DP83867IR 可以PING通,但是无法和LINUX的核心板通信

Part Number: DP83867IR

TI原厂:

你们好,我新画的DP83867底板和LINUX核心板联调,千兆网口无法和XSHELL通信(测试3.3V,2.5V,1.0V电源都是正常的)。

想请教PING通之后,还需要重点查看调试哪块电路,LINUX核心板和以前别的验证过是好用的。

1.调试记录

用wireshark 抓和LINUX的信息

最后一直ARP询问

最后绿灯常亮

可以ping通

 

2.下面位原理图和PCB,其中带DNP_前缀的都需要焊掉