Other Parts Discussed in Thread: DS90CR286A
你好,最近在做CAMERALINK接口,选择了DS90CR288A这颗转换芯片,发现他是-10℃~70℃,现在要求是-40℃~85℃,
1、请问是否有相应的推荐器件,同时是否有参开设计
2、CAMERALINK信号(数据与控制)能否直接进FPGA接口
谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,最近在做CAMERALINK接口,选择了DS90CR288A这颗转换芯片,发现他是-10℃~70℃,现在要求是-40℃~85℃,
1、请问是否有相应的推荐器件,同时是否有参开设计
2、CAMERALINK信号(数据与控制)能否直接进FPGA接口
谢谢。
感谢您对TI产品的关注!
关于你的咨询,现在的catalog中与DS90CR288A相近的只有DS90CR286A是-40 to 85, 但它是66 MHz的
www.ti.com/.../DS90CR286A
CAMERALINK信号是通过多条串行线传输的,可以直接连接到FPGA接口,但是需要注意以下几点:
确保CAMERALINK信号的电平与FPGA兼容。如果需要,采用电平转换芯片。
FPGA需要具备适配CAMERALINK工作速率的时序特性。
使用FPGA进行CAMERALINK信号处理时,可能需要额外的设计工作,包括编写合适的Verilog/VHDL代码,实现对CAMERALINK协议的解析和处理。
请了解。