Other Parts Discussed in Thread: TCAN4550
There is no oscillation signal on the crystal, the design circuit is as shown in the figure, VCCout has 5V signal, Vio=3.3V, does EP suspension have any effect? Replace TCAN4500, crystal, and C27, C30 (10p, 12p,15p,18p,20p) have no oscillation signal,when R58=680K C27=C30=12pf , there is an oscillation signal, but the frequency is 71KHz or so, also incorrect.