This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS250DF810: link could not establish

Part Number: DS250DF810

dears,

My customer used DS250DF810 between the switch chip CTC7132 and the optical module. The hardware connection block diagram is as below:

The test environment: the optical port is self-looped through the optical fiber. 

The register configuration is as below:

->retimer_bpo_cfg 10

->0xffffffff (ShadowTask):1970-01-01 02:37:55<interrupt>[-1]: TEST           -MAJOR        set array[0]: reg = 0xfc, value = 0x1

0xffffffff (ShadowTask):1970-01-01 02:37:55<interrupt>[-1]: TEST           -MAJOR        set array[1]: reg = 0xff, value = 0x3

0xffffffff (ShadowTask):1970-01-01 02:37:55<interrupt>[-1]: TEST           -MAJOR        set array[2]: reg = 0x0, value = 0x4

0xffffffff (ShadowTask):1970-01-01 02:37:55<interrupt>[-1]: TEST           -MAJOR        set array[3]: reg = 0xa, value = 0xc

0xffffffff (ShadowTask):1970-01-01 02:37:55<interrupt>[-1]: TEST           -MAJOR        set array[4]: reg = 0x60, value = 0x27

0xffffffff (ShadowTask):1970-01-01 02:37:55<interrupt>[-1]: TEST           -MAJOR        set array[5]: reg = 0x61, value = 0xb1

0xffffffff (ShadowTask):1970-01-01 02:37:55<interrupt>[-1]: TEST           -MAJOR        set array[6]: reg = 0x62, value = 0x27

0xffffffff (ShadowTask):1970-01-01 02:37:55<interrupt>[-1]: TEST           -MAJOR        set array[7]: reg = 0x63, value = 0xb1

0xffffffff (ShadowTask):1970-01-01 02:37:55<interrupt>[-1]: TEST           -MAJOR        set array[8]: reg = 0x64, value = 0xff

0xffffffff (ShadowTask):1970-01-01 02:37:55<interrupt>[-1]: TEST           -MAJOR        set array[9]: reg = 0x9, value = 0x4

0xffffffff (ShadowTask):1970-01-01 02:37:55<interrupt>[-1]: TEST           -MAJOR        set array[10]: reg = 0x18, value = 0x10

0xffffffff (ShadowTask):1970-01-01 02:37:55<interrupt>[-1]: TEST           -MAJOR        set array[11]: reg = 0x31, value = 0x40

0xffffffff (ShadowTask):1970-01-01 02:37:55<interrupt>[-1]: TEST           -MAJOR        set array[12]: reg = 0x1e, value = 0xe3

0xffffffff (ShadowTask):1970-01-01 02:37:55<interrupt>[-1]: TEST           -MAJOR        set array[13]: reg = 0x3d, value = 0x9a

0xffffffff (ShadowTask):1970-01-01 02:37:55<interrupt>[-1]: TEST           -MAJOR        set array[14]: reg = 0x3f, value = 0x40

0xffffffff (ShadowTask):1970-01-01 02:37:55<interrupt>[-1]: TEST           -MAJOR        set array[15]: reg = 0x3e, value = 0x40

0xffffffff (ShadowTask):1970-01-01 02:37:55<interrupt>[-1]: TEST           -MAJOR        set array[16]: reg = 0x3d, value = 0x8d

0xffffffff (ShadowTask):1970-01-01 02:37:55<interrupt>[-1]: TEST           -MAJOR        set array[17]: reg = 0x3f, value = 0x42

0xffffffff (ShadowTask):1970-01-01 02:37:55<interrupt>[-1]: TEST           -MAJOR        set array[18]: reg = 0x3e, value = 0x41

0xffffffff (ShadowTask):1970-01-01 02:37:55<interrupt>[-1]: TEST           -MAJOR        set array[19]: reg = 0xa, value = 0x0

value = 0 = 0x0

the DF810 chip ID is read normally, the value of the 0x78 register is read as 0x20, the value of the 0x27 and 28 registers is read as 0x0, and the switch main chip feedback that the LINK to the optical module  is not establish. the issue occurs after the CTC7132 and retimer are configured.

the customer used DS250DF810 previously and it may work normally. the issue happens after change the switch chip to CTC7132 (there is no any other change). The switching chip has been configured normally.  The customer use the DS250DF810 configuration file of the previous mass-produced project. the register of DF810 is attached below: 

dd_retimer_readall_debug 0
0xffffffff (ShadowTask):Global{Reg,Value}:  {0xef,0xc}  {0xf0,0x32}  {0xf1,0x10}  {0xf3,0x0}  {0xfb,0x4} {0xfc,0x0} {0xfd,0x0} {0xfe,0x3} {0xff,0x0}
0xffffffff (ShadowTask):select Share Quad1, set {0xff,0x20}
0xffffffff (ShadowTask):Share Quad1{Reg,Value}:  {0x0,0x0}  {0x1,0x50}  {0x2,0x0}  {0x3,0x0}  {0x4,0x9} {0x5,0x1} {0x6,0x0} {0x8,0x0} {0xa,0x0}  {0xb,0x40}  {0xc,0x0}  {0xd,0x42}  {0xe,0x3}  {0xf,0x0} {0x10,0xff} {0x11,0x0} {0x12,0x91}
0xffffffff (ShadowTask):select Share Quad0, set {0xff,0x10}
0xffffffff (ShadowTask):Share Quad0{Reg,Value}:  {0x0,0x0}  {0x1,0x50}  {0x2,0x0}  {0x3,0x0}  {0x4,0x9} {0x5,0x1} {0x6,0x0} {0x8,0x0} {0xa,0x0}  {0xb,0x40}  {0xc,0x0}  {0xd,0xb4}  {0xe,0x1}  {0xf,0x0} {0x10,0xff} {0x11,0x0} {0x12,0x91}
0xffffffff (ShadowTask):select channel[0], set {0xfc,0x1} {0xff,0x01}
0xffffffff (ShadowTask):Channel{Reg,Value}:  {0x0,0x0} {0x1,0x80} {0x2,0x1}  {0x3,0x0} {0x4,0x1} {0x5,0x1} {0x6,0x1} {0x7,0x1}   {0x8,0x73} {0x9,0x0} {0xa,0x0} {0xb,0x63} {0xc,0x0} {0xd,0x80} {0xe,0x93} {0xf,0x69}
0xffffffff (ShadowTask):Channel{Reg,Value}:  {0x10,0x0} {0x11,0x20} {0x12,0x83}  {0x13,0xb0} {0x14,0x4} {0x15,0x10} {0x16,0x7a} {0x17,0x36}   {0x18,0x40} {0x19,0x20} {0x1a,0x58} {0x1b,0x3} {0x1c,0x90} {0x1d,0x0} {0x1e,0xe9} {0x1f,0xb}
0xffffffff (ShadowTask):Channel{Reg,Value}:  {0x20,0x0} {0x21,0x0} {0x22,0x0}  {0x23,0x40} {0x24,0x40} {0x25,0x0} {0x26,0x0} {0x27,0x0}   {0x28,0x0} {0x29,0x3} {0x2a,0x5a} {0x2b,0xa} {0x2c,0xf6} {0x2d,0x30} {0x2e,0x0} {0x2f,0x54}
0xffffffff (ShadowTask):Channel{Reg,Value}:  {0x30,0x0} {0x31,0x20} {0x32,0x11}  {0x33,0x88} {0x34,0xbf} {0x35,0xf} {0x36,0x30} {0x37,0x5}   {0x38,0x0} {0x39,0x60} {0x3a,0x0} {0x3b,0x3f} {0x3c,0x6b} {0x3d,0x1a} {0x3e,0x40} {0x3f,0x40}
0xffffffff (ShadowTask):Channel{Reg,Value}:  {0x40,0x0} {0x41,0x40} {0x42,0x50}  {0x43,0x80} {0x44,0x90} {0x45,0xc0} {0x46,0xd0} {0x47,0xd1}   {0x48,0xd5} {0x49,0xd8} {0x4a,0xea} {0x4b,0xf7} {0x4c,0xfd} {0x4d,0xee} {0x4e,0xef} {0x4f,0xff}
0xffffffff (ShadowTask):Channel{Reg,Value}:  {0x50,0x0} {0x51,0x0} {0x52,0x0}  {0x53,0x0} {0x54,0x0} {0x55,0x0} {0x56,0x0} {0x57,0x0}   {0x58,0x0} {0x59,0x0} {0x5a,0x0} {0x5b,0x0} {0x5c,0x0} {0x5d,0x0} {0x5e,0x0} {0x5f,0x0}
0xffffffff (ShadowTask):Channel{Reg,Value}:  {0x60,0x0} {0x61,0x0} {0x62,0x0}  {0x63,0x0} {0x64,0x0} {0x65,0x0} {0x66,0x0} {0x67,0x20}   {0x68,0x0} {0x69,0xa} {0x6a,0x21} {0x6b,0x40} {0x6c,0x0} {0x6d,0x0} {0x6e,0x0} {0x6f,0x0}
0xffffffff (ShadowTask):Channel{Reg,Value}:  {0x70,0x5} {0x71,0x23} {0x72,0x0}  {0x73,0x0} {0x74,0x0} {0x75,0x0} {0x76,0x21} {0x77,0x1a}   {0x78,0x20} {0x79,0x10} {0x7a,0x0} {0x7b,0x0} {0x7c,0x0} {0x7d,0x48} {0x7e,0x13} {0x7f,0x2a}
0xffffffff (ShadowTask):Channel{Reg,Value}:  {0x80,0x0} {0x81,0xe5} {0x82,0x0}  {0x83,0x1} {0x84,0x0} {0x85,0x0} {0x86,0x0} {0x87,0x0}   {0x88,0x0} {0x89,0x0} {0x8a,0x0} {0x8b,0x0} {0x8c,0x0} {0x8d,0x0} {0x8e,0x0} {0x8f,0x0}
0xffffffff (ShadowTask):Channel{Reg,Value}:  {0x90,0x0} {0x91,0x0} {0x92,0x0}  {0x93,0x0} {0x94,0x0} {0x95,0x0} {0x96,0x8} {0x97,0xff}   {0x98,0x0} {0x99,0x3f} {0x9a,0x3f} {0x9b,0xe0} {0x9c,0x24} {0x9d,0xa5} {0x9e,0x48} {0x9f,0x0}
0xffffffff (ShadowTask):Channel{Reg,Value}:  {0xa0,0x0} {0xa1,0x40} {0xa2,0x50}  {0xa3,0x80} {0xa4,0x90} {0xa5,0x20} {0xa6,0x43} {0xa7,0xdf}   {0xa8,0x0} {0xa9,0x0}
value = 0 = 0x0


retimer_sct_cfg 0,10
0xffffffff (ShadowTask):1970-01-01 00:08:07<interrupt>[-1]: TEST           -MAJOR        set array[0]: reg = 0xff, value = 0x1
0xffffffff (ShadowTask):1970-01-01 00:08:07<interrupt>[-1]: TEST           -MAJOR        set array[0]: reg = 0xfc, value = 0x1
0xffffffff (ShadowTask):1970-01-01 00:08:07<interrupt>[-1]: TEST           -MAJOR        set array[0]: reg = 0xff, value = 0x1
0xffffffff (ShadowTask):1970-01-01 00:08:07<interrupt>[-1]: TEST           -MAJOR        set array[1]: reg = 0xfc, value = 0x1
0xffffffff (ShadowTask):1970-01-01 00:08:07<interrupt>[-1]: TEST           -MAJOR        set array[2]: reg = 0x0, value = 0x4
0xffffffff (ShadowTask):1970-01-01 00:08:07<interrupt>[-1]: TEST           -MAJOR        set array[3]: reg = 0xa, value = 0xc
0xffffffff (ShadowTask):1970-01-01 00:08:07<interrupt>[-1]: TEST           -MAJOR        set array[4]: reg = 0x60, value = 0x90
0xffffffff (ShadowTask):1970-01-01 00:08:07<interrupt>[-1]: TEST           -MAJOR        set array[5]: reg = 0x61, value = 0xb3
0xffffffff (ShadowTask):1970-01-01 00:08:07<interrupt>[-1]: TEST           -MAJOR        set array[6]: reg = 0x62, value = 0x90
0xffffffff (ShadowTask):1970-01-01 00:08:07<interrupt>[-1]: TEST           -MAJOR        set array[7]: reg = 0x63, value = 0xb3
0xffffffff (ShadowTask):1970-01-01 00:08:07<interrupt>[-1]: TEST           -MAJOR        set array[8]: reg = 0x64, value = 0xff
0xffffffff (ShadowTask):1970-01-01 00:08:07<interrupt>[-1]: TEST           -MAJOR        set array[9]: reg = 0x9, value = 0x4
0xffffffff (ShadowTask):1970-01-01 00:08:07<interrupt>[-1]: TEST           -MAJOR        set array[10]: reg = 0x18, value = 0x10
0xffffffff (ShadowTask):1970-01-01 00:08:07<interrupt>[-1]: TEST           -MAJOR        set array[11]: reg = 0x31, value = 0x40
0xffffffff (ShadowTask):1970-01-01 00:08:07<interrupt>[-1]: TEST           -MAJOR        set array[12]: reg = 0x1e, value = 0xe3
0xffffffff (ShadowTask):1970-01-01 00:08:07<interrupt>[-1]: TEST           -MAJOR        set array[13]: reg = 0x3d, value = 0x9a
0xffffffff (ShadowTask):1970-01-01 00:08:07<interrupt>[-1]: TEST           -MAJOR        set array[14]: reg = 0x3d, value = 0x9a
0xffffffff (ShadowTask):1970-01-01 00:08:07<interrupt>[-1]: TEST           -MAJOR        set array[15]: reg = 0x3f, value = 0x40
0xffffffff (ShadowTask):1970-01-01 00:08:07<interrupt>[-1]: TEST           -MAJOR        set array[16]: reg = 0x3e, value = 0x40
0xffffffff (ShadowTask):1970-01-01 00:08:07<interrupt>[-1]: TEST           -MAJOR        set array[17]: reg = 0x3d, value = 0x8a
0xffffffff (ShadowTask):1970-01-01 00:08:08<interrupt>[-1]: TEST           -MAJOR        set array[18]: reg = 0x3f, value = 0x41
0xffffffff (ShadowTask):1970-01-01 00:08:08<interrupt>[-1]: TEST           -MAJOR        set array[19]: reg = 0x3e, value = 0x41
0xffffffff (ShadowTask):1970-01-01 00:08:08<interrupt>[-1]: TEST           -MAJOR        set array[20]: reg = 0xa, value = 0x0
value = 0 = 0x0

->
->
->dd_retimer_readall_debug 0
->0xffffffff (ShadowTask):Global{Reg,Value}:  {0xef,0xc}  {0xf0,0x32}  {0xf1,0x10}  {0xf3,0x0}  {0xfb,0x4} {0xfc,0x1} {0xfd,0x0} {0xfe,0x3} {0xff,0x1}
0xffffffff (ShadowTask):select Share Quad1, set {0xff,0x20}
0xffffffff (ShadowTask):Share Quad1{Reg,Value}:  {0x0,0x0}  {0x1,0x50}  {0x2,0x0}  {0x3,0x0}  {0x4,0x9} {0x5,0x1} {0x6,0x0} {0x8,0x0} {0xa,0x0}  {0xb,0x40}  {0xc,0x0}  {0xd,0x42}  {0xe,0x3}  {0xf,0x0} {0x10,0xff} {0x11,0x0} {0x12,0x91}
0xffffffff (ShadowTask):select Share Quad0, set {0xff,0x10}
0xffffffff (ShadowTask):Share Quad0{Reg,Value}:  {0x0,0x0}  {0x1,0x50}  {0x2,0x0}  {0x3,0x0}  {0x4,0x9} {0x5,0x1} {0x6,0x0} {0x8,0x0} {0xa,0x0}  {0xb,0x40}  {0xc,0x0}  {0xd,0xb4}  {0xe,0x1}  {0xf,0x0} {0x10,0xff} {0x11,0x0} {0x12,0x91}
0xffffffff (ShadowTask):select channel[0], set {0xfc,0x1} {0xff,0x01}
0xffffffff (ShadowTask):Channel{Reg,Value}:  {0x0,0x0} {0x1,0x80} {0x2,0x0}  {0x3,0x0} {0x4,0x1} {0x5,0x1} {0x6,0x1} {0x7,0x1}   {0x8,0x73} {0x9,0x4} {0xa,0x0} {0xb,0x63} {0xc,0x0} {0xd,0x80} {0xe,0x93} {0xf,0x69}
0xffffffff (ShadowTask):Channel{Reg,Value}:  {0x10,0x0} {0x11,0x20} {0x12,0x83}  {0x13,0xb0} {0x14,0x4} {0x15,0x10} {0x16,0x7a} {0x17,0x36}   {0x18,0x10} {0x19,0x20} {0x1a,0x58} {0x1b,0x3} {0x1c,0x90} {0x1d,0x0} {0x1e,0xe3} {0x1f,0xb}
0xffffffff (ShadowTask):Channel{Reg,Value}:  {0x20,0x0} {0x21,0x0} {0x22,0x0}  {0x23,0x40} {0x24,0x40} {0x25,0x0} {0x26,0x0} {0x27,0x0}   {0x28,0x0} {0x29,0x3} {0x2a,0x5a} {0x2b,0xa} {0x2c,0xf6} {0x2d,0x30} {0x2e,0x0} {0x2f,0x54}
0xffffffff (ShadowTask):Channel{Reg,Value}:  {0x30,0x0} {0x31,0x40} {0x32,0x11}  {0x33,0x88} {0x34,0xbf} {0x35,0xf} {0x36,0x30} {0x37,0x9}   {0x38,0x0} {0x39,0x60} {0x3a,0x0} {0x3b,0x32} {0x3c,0xe6} {0x3d,0x8a} {0x3e,0x41} {0x3f,0x41}
0xffffffff (ShadowTask):Channel{Reg,Value}:  {0x40,0x0} {0x41,0x40} {0x42,0x50}  {0x43,0x80} {0x44,0x90} {0x45,0xc0} {0x46,0xd0} {0x47,0xd1}   {0x48,0xd5} {0x49,0xd8} {0x4a,0xea} {0x4b,0xf7} {0x4c,0xfd} {0x4d,0xee} {0x4e,0xef} {0x4f,0xff}
0xffffffff (ShadowTask):Channel{Reg,Value}:  {0x50,0x0} {0x51,0x0} {0x52,0x0}  {0x53,0x0} {0x54,0x0} {0x55,0x0} {0x56,0x0} {0x57,0x0}   {0x58,0x0} {0x59,0x0} {0x5a,0x0} {0x5b,0x0} {0x5c,0x0} {0x5d,0x0} {0x5e,0x0} {0x5f,0x0}
0xffffffff (ShadowTask):Channel{Reg,Value}:  {0x60,0x90} {0x61,0xb3} {0x62,0x90}  {0x63,0xb3} {0x64,0xff} {0x65,0x0} {0x66,0x0} {0x67,0x20}   {0x68,0x0} {0x69,0xa} {0x6a,0x21} {0x6b,0x40} {0x6c,0x0} {0x6d,0x0} {0x6e,0x0} {0x6f,0x0}
0xffffffff (ShadowTask):Channel{Reg,Value}:  {0x70,0x5} {0x71,0x23} {0x72,0x0}  {0x73,0x0} {0x74,0x0} {0x75,0x0} {0x76,0x21} {0x77,0x1a}   {0x78,0x20} {0x79,0x10} {0x7a,0x0} {0x7b,0x0} {0x7c,0x0} {0x7d,0x48} {0x7e,0x13} {0x7f,0x2a}
0xffffffff (ShadowTask):Channel{Reg,Value}:  {0x80,0x0} {0x81,0xe5} {0x82,0x0}  {0x83,0x1} {0x84,0x0} {0x85,0x0} {0x86,0x0} {0x87,0x0}   {0x88,0x0} {0x89,0x0} {0x8a,0x0} {0x8b,0x0} {0x8c,0x0} {0x8d,0x0} {0x8e,0x0} {0x8f,0x90}
0xffffffff (ShadowTask):Channel{Reg,Value}:  {0x90,0x0} {0x91,0x0} {0x92,0x0}  {0x93,0x0} {0x94,0x0} {0x95,0x0} {0x96,0x8} {0x97,0xff}   {0x98,0x0} {0x99,0x3f} {0x9a,0x3f} {0x9b,0xe0} {0x9c,0x24} {0x9d,0xa5} {0x9e,0x48} {0x9f,0x0}
0xffffffff (ShadowTask):Channel{Reg,Value}:  {0xa0,0x0} {0xa1,0x40} {0xa2,0x50}  {0xa3,0x80} {0xa4,0x90} {0xa5,0x20} {0xa6,0x43} {0xa7,0xdf}   {0xa8,0x0} {0xa9,0x0}
value = 0 = 0x0

if bypass CDR after writing the registers of retimer, the port connected to the 4 optical ports  can be Linked up with CTC7132.

would you please help to guide the customer how to resolve the issue?

thnaks a lot!