Part Number: DS90UB983-Q1
983能跟688配合使用吗,屏端688配置的模式是6.5G,Dual OLDI outpu、FPD4 Auto-detect
我看688的数据手册介绍向后兼容983的FPD-LINK III模式,实时真的是这样吗
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB983-Q1
983能跟688配合使用吗,屏端688配置的模式是6.5G,Dual OLDI outpu、FPD4 Auto-detect
我看688的数据手册介绍向后兼容983的FPD-LINK III模式,实时真的是这样吗
是的,DS90UB983可以在FPD Link IV 6.75Gbps操作中与DS90UB688配合使用。
是的,983还具有向后兼容性,可以在FPD Link III模式下运行。此FPD链路模式应通过您显示的引脚绑定进行设置,也可以在FPD4_RX_CFG寄存器0x31[4:0]中覆盖。当通过FPD链路使用I2C实时更改FPD链路速率时,请在更改Ser设置之前更改Des FPD链路设置。一旦Ser和Des具有匹配的配置,FPD链路应重新锁定。
983端我配置的是FPD IV 6.75Gbps、Single Port 0,688端配置的是6.5G,Dual OLDI outpu、FPD4 Auto-detect,983端读取寄存器0x0C = 0x03,可以监测到线路LINK上,但是读取寄存器0x08 = 0x00,识别不到,正常线路连接上Ser不是可以自动识别Deser短的I2C地址吗,我这个识别不出来是配置的不对吗
下面是688端引脚配置
//MODE_SEL0 = 0.587V FPD4 Auto-detect
//MODE_SEL2 = 1V Daisy-Chain OFF
//MODE_SEL1 = 0.79V Dual OLDI SWAP output