This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2571使用问题

Other Parts Discussed in Thread: LMX2571, LMX2581, CLOCKDESIGNTOOL, LMX2572

关于LMX2571的使用,我们有一些疑问想请教一下。

    1.这款芯片具有FSK调制功能,和我们想使用的GMSK两点调制不太一样,不知道怎么将调制信号加载到VCO上去,另外 SPI 编程、I2S 编程和 PIN 模式编程不知道对GMSK两点调制有什么用。问题一是怎么将调制信号加载到VCO上去,哪些编程模式对我是否有用。

   2.问题2是关于环路带宽设置的问题。由于它是小数分频器件,PDF可以很大,我们设计的是12.8MHz,输出步进是12.5KHz,输出频率是860MHz--940MHz,那么这时候环路滤波器的带宽怎么设置才好呢?以前使用的是整数分频,对这个没有经验。

  3. 我要用这个器件做时分复用的中继站的本振源和载波,方案是否可行?

谢谢!

  • 你好,

    Q3: LMX2581更适合基站应用中的本振源,相比LMX2571有更好的相噪性能。LMX2571定位定功耗应用。

    Q2:这个问题太负责,需要用户自习学习相关的小数分频理论,推荐TI官网的一篇应用文章作。

    http://www.ti.com/general/docs/lit/getliterature.tsp?baseLiteratureNumber=snaa062

    Q1:LMX2571的FSK调制功能需要主芯片支持I2S接口的调制输出接口,对于IC集成了VCO的方案,通常不支持VCO调制,推荐参考信号调制方案。

  • 总结更正下,1.调制信号是通过可以选择的三种方式直接调制VCO上:pin mode, SP mode, I2S MODE具体使用方法参考手册12~36页。

    2.环路设置需要根据你的频率仿真确定,请使用 clock design tool,官网下载。

    http://www.ti.com/tool/clockdesigntool?keyMatch=clock%20design%20tool&tisearch=Search-EN-Everything

    3.一般的数字中继,直放站都不会使用直接调制,直接变频数模转换,数字处理,然后再模数转换,功放输出。请提供你的设计方案

  • 你好,请教一下,LMX2571 加4FSK调制,走的是I2S接口,调制出来的频谱很宽,邻道功率不合格呀,你们自己测过吗?

  • 4FSK数据需要经过FIR滤波后才能发给2571的I2S,否则频谱扩展。

    测试过,请留下联系方式或与我们直接联系,谢谢

  • 您好,我们用的96KHz的调制速率,调制出来的波形在offset 96KHz处有杂散且有调制,请问你们遇到没有这种问题没?有的话怎么解决的?

  • Hi Mark

    如果采I2S接口进行调制的话,对于数字对讲机应用的,时钟为96khz的话,杂散大概在-70dBc的水平,如果提高一倍I2S_CLK,比如192kHz,杂散提高10dB左右,这是客户的实测结果,供参考。

  • 您好,我想请教一下LMX2572的使用,在FSK SPI 或 FSK FAST SPI模式下,FSK的数据流怎么注入,是直接输入到SPI的三个管脚吗?还是通过DSP芯片,根据0或1电平改写切换LMX2572的寄存器内容?

  • 对于I2S接口调制,发送的调制数据是频偏吗?